This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HalCoGen support for CAN remote frame reception?

Other Parts Discussed in Thread: HALCOGEN

Hi,

How do you enable CAN Remote Enable (bit 9 in IF1/IF2 Message Control Register) using HALCoGen?

Thanks,

Mandeep

  • Hi Mandeep,

    I see that HALCoGen today does not support setting the RmtEn control bit. I will let the HALCoGen tool development team know so that this can be added in a future update of the tool. In the mean time, you can add your own code to write to the IF1/2 MCTL control register to set the RmtEn bit. Please remember to add the code inside the 

    /* USER CODE BEGIN (5) */
    /* USER CODE END */

    You will also have to enable the CAN module initialization mode before writing to the MCTL register, and then also exit the initialization mode.

    Regards, Sunil