This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to toggle T-BIT of CPSR using GEL script

Hello Support,

Can you please provide some concrete example of GEL Script with which I can change between ARM and THUMB mode dynamically?

Thank you.
Regards
Pashan

  • Hello,

    There is no way to embed assembly instructions inside a gel function. However, you can write a javascript routine that uses the eval function to set the CPSR to the value that you want (including updating the T bit).

    You can then add a "hotmenu" to the Scripts menu option by using the "hotmenu_addJSFunction" javascript command. I can try to put together an example for you later today using this procedure.

    Regards,

    Sunil