Hi
I have a RDK - BLDC and some MDL - BLDC devices. Somehow it's not possible to connect over ethernet to the MDL - BLDC devices with the BLDC GUI. When starting up the gui it always tries to connect to the ip of the mdl - bldc device and fails. With an IP scann I didn't find the device in the ip range of the dhcp server ether . Actually I got an answer on 169.254.89.71 like described in the provided manual but unfortunately I was still not able to connect with the BLDC Gui programm in this ip range.
What can I do? I tried it with a new device and with a manually updated device from the qs-bldc project provided from the StellarisWare. How can I reset the last connected ip address.
Thank you for helping me.