Other Parts Discussed in Thread: TMS570LS3137
Hello,
I have to transmit data between two TMS570LS3137 via SCI. I decided to use DMA to decrease CPU load.
Therefore I want to trigger the DMA tx request by SW.
My question is, how can I trigger it or in other words, which bit do I have to set, to trigger a SCI DMA transmission.
Here is my init code, maybe I have forgotten something important:
SCI2Init(); // contains SET_TX_DMA enable
// bring DMA out of reset
DMAGCTRL_bit.DMA_RES = 1U;
// init Control-Packets
DMA_CPClear();
// activate DMA
DMAGCTRL_bit.DMA_EN = 1U;
DMAGCTRL_bit.DEBUG_MODE = 0x03;
DMACP0ISADDR = (unsigned int)&dataArray; /* SRCADDR is the MIBSPI3 RX Buffer */
DMACP0IDADDR = (unsigned int)&SCI2TD; /* DSTADDR is the address of dataArray */
DMACP0ITCOUNT_bit.IFTCOUNT = 1; /* FRM_CNT 1 Frame transfer */
DMACP0ITCOUNT_bit.IETCOUNT = 27; /* 27 Elements per Frame */
DMACP0CHCTRL_bit.RES = ACCESS_8_BIT; /* RD_SIZE Size of source element */
DMACP0CHCTRL_bit.WES = ACCESS_8_BIT; /* WR_SIZE Size of destination element */
DMACP0CHCTRL_bit.TTYPE = FRAME_TRANSFER; /* TRANSFER_TYPE */
DMACP0CHCTRL_bit.ADDMR = ADDR_FIXED; //ADDR_INC1; /* RD_ADDR_MODE Auto increment src (read) */
DMACP0CHCTRL_bit.ADDMW = ADDR_FIXED;
DMACP0CHCTRL_bit.AIM = AUTOINIT_OFF; /* AUTOINIT Disable */
DMACP0EIOFF_bit.EIDXD = 0; /* ELM_DST_OFFST (for Index mode) */
DMACP0EIOFF_bit.EIDXS = 0; /* ELM_SRC_OFFST (for Index mode) */
DMACP0FIOFF_bit.EIDXD = 0; /* FRM_DST_OFFST (for Index mode) */
DMACP0FIOFF_bit.EIDXS = 0; /* FRM_SRC_OFFST (for Index mode) */
DMACP0CHCTRL_bit.CHAIN = 0; /* channel Ctrl info by default NO Channing is Enabled.*/
DMAPAR0_bit.CH0PA = PORTB;
//Bypass FIFO
DMAPTCRL_bit.BYB = 1U;
//Configuring the DMA Request Register
//i.e Mapping the DMA Channel request to DMA Channel
DMADREQASI0_bit.CH0ASI = 31;
//Enable Trigger for Channel 0
DMAHWCHENAS_bit.HWCHENA0 = 1U;
Thanks in advance,
Fuchs Dominik