Other Parts Discussed in Thread: DRV8301
When I enable the motor controller via the gui->EnableFlg of the Motorware foc_encoder_speed example of the DRV8301 RM48 kit, I can see a periodic noise (much like the pwms) on the pins SCI_RX (DIMM 74), LIN_RX (SCIRX_Base, DIMM 43), QEPA (DIMM 40) etc., via an oscilloscope. Because of the noise, the SCI module keeps getting parity errors, thus the constant losing of packets. Do you have any suggestions for solving this noise problem of the DRV8301 RM48 kit? It only appears after I enable the motor controller by setting gui->EnableFlg.