Other Parts Discussed in Thread: TM4C123GH6PGE
After installation of "SW-TM4C-1.0.exe" to get the "TivaWare_C_Series-1.0" directory in parallel to the old "StellarisWare" directory I tried to build the "blinky" demo.
1.
After copy of "boards" directory from StellarisWare to the TivaWare directory I had to change the "blinky.c" file.
#include "inc/tm4c123gh6pge.h"
2.
The register and masks definition file tm4c123gh6pge.h needs new type definition for the C99 types.
>notepad c:\ti\TivaWare_C_Series-1.0\inc\tm4c123gh6pge.h
#ifndef __TM4C123GH6PGE_H__
#define __TM4C123GH6PGE_H__
#include <stdint.h>
#include <stdbool.h>
3.
In the project properties under C/C++ Build | Settings | Build Steps | Post-build steps:
rename ofd470 into armofd and hex470 into armhex
(or double the post-build tools in c:\ti\ccsv5\tools\compiler\arm_5.0.4\bin\)
After that a working image could be produced in c:\ti\My Workspace\blinky\Debug\
These steps are necessary for all other demos. So my question is:
Can TI provide a new firmware version for the evaluation kit that regards the new naming?