Other Parts Discussed in Thread: HALCOGEN, RM48L952, TMS570LS3137
Hi,
I'm having trouble using DMA to read MibSPI rx buffers. Attached is my current code:6013.test.zip
Here is a screenshot after transfer is complete:
Esentially, two 16 bit bytes have been received: 0x0FFF and 0x0D4A. Note that the memory view on the right shows the mibSPI1 RX buffer. RX_DATA, which uses DMA to transfer from mibSPI RAM to RAM, (see value in watch) is missing the second byte, whilst RX_DATA2 (which uses mibspiGetData() as in the mibSPI example code) contains the correct two bytes as confirmed with a scope. So, the SPI is working, but DMA copy to RAM is not.
Please take a look at my code and see if anything is wrong. Also, I have a question - what is the function of R(T)XDMA_MAPx? I thought MIBSPI[1] request source is hardwired to DMAREQ[0]?