Other Parts Discussed in Thread: HALCOGEN
Hi,
I'm working on a TMDX570LS31HDK. Multi buffered SPI (MibSPI5) can be used in parallel 8 mode so the ouput should use 8 pins for SOMI lines 0 to 7.
In HalCoGe (in the MibSPI5 and in mux tabs) and in the user manual pin description there are SOMI lines only from 0 to 3.
Where are the others?
Can the TMDX570LS31HDK use 8 parallel mode or this is reserved to other HW models?
Grazie,
Matteo