Other Parts Discussed in Thread: HALCOGEN
Hello,
I recently received a new TMDXRM48HDK for continued prototype development (our previous HDK was broken during testing).
The application that was previously working on our other HDK throws ESM errors on the new board. The new board has never been tested with external IO (source of previous failure). I am seeing intermittent success with running the board with the application we developed, also with the demo applications that come with the HDK.
To try and debug the problem I have tried to generate from HALcogen empty applications with only the GIO enabled and toggle the NHET pins in the main loop. This has had intermittent success, with ESM errors occurring frequently. If I do anything more advanced such as enabling a HET driver and trying to both PWM a HET pin and, say, use another as GIO I end up with ESM errors.
Can anyone help me debug the source of the ESM error in the event there is a chance it could be an initialization issue with the micro? I think it is unlikely and we may have been shipped a defective board.
Thanks
Jamie