Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSV5.4.00091-Linux 'config is not defined'

I began to try CCSV5.3 on Windows with LM4F120 board. Runs example from TI-RTOS 1.01 without issue. However, my company default develop environment is Linux. So I install CCSV5.4. The same example has compilation errors. The message is 

xs.js: xdc.Warnings failure: package path: /opt/ti/tirtos_1_01_00_25/packages;/opt/ti/tirtos_1_01_00_25/products/bios_6_34_04_22/packages;/opt/ti/tirtos_1_01_00_25/products/ipc_1_25_02_12/packages;/opt/ti/tirtos_1_01_00_25/products/ndk_2_22_01_14/packages;/opt/ti/tirtos_1_01_00_25/products/uia_1_02_00_07/packages;/opt/ti/tirtos_1_01_00_25/products/xdctools_3_24_06_63/packages;/opt/ti/ccsv5/ccs_base;/opt/ti/xdctools_3_25_00_48/packages;..;
js: "/opt/ti/tirtos_1_01_00_25/products/xdctools_3_24_06_63/packages/xdc/bld/BuildEnvironment.xs", line 146: ReferenceError: "config" is not defined.
gmake: *** No rule to make target `.configuro'. Stop.
js: "/opt/ti/tirtos_1_01_00_25/products/xdctools_3_24_06_63/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
"/opt/ti/tirtos_1_01_00_25/products/xdctools_3_24_06_63/packages/xdc/tools/configuro/Main.xs", line 74
"/opt/ti/tirtos_1_01_00_25/products/xdctools_3_24_06_63/packages/xdc/tools/ICmd.xs", line 50

I reinstall the CCS and it doesn't seems have any effect. Did I miss anything or there are difference between Linux and Windows version.

Thanks

Tony

  • Hi Tony,

    is this the launchpad? I ask because I know that the launchpad is not officially supported on Linux. There are a few sites that might help you but it is a bit hacky and not guaranteed.

    http://hackaday.com/2012/10/29/guide-to-developing-with-the-stellaris-launchpad-on-a-linux-box/

    http://www.jann.cc/2012/12/11/getting_started_with_the_ti_stellaris_launchpad_on_linux.html

    Please keep us informed.

    Best Regards,
    Lisa

  • Hi,

    It''s lunchpad. However, I was told that CCSV5 support Linux. and the process failed at the compiling stage, not the actual debugging/USB connection stage. Guess I will need to stick with windows for a while if I can't find the solution. 

    Tony

  • Hi Tony,

    yes, ccsv5 runs on Linux, however, unfortunately some devices like the stellaris and msp430 original launchpads are not (at least not yet) supported. 

    Sorry for any inconvenience.  If you have a windows pc, I suspect your launchpad will be easy to get up and running.  Please keep us informed.

    Best Regards,

    Lisa

  • Hi,

    I thought it's Linux issue. But after I upgrade my windows environment from 5.3 to 5.4. I got the same issue. Actually, I just searched the forum. There is other post that also has same issue with different MPU. It's more like TI-RTOS/CCS integration problem. You can search 'CCSv5.4' and 'config' you will see. (I found one posted by john3909).

    Please help us on this issue. I can't keep TI-RTOS stuff going and I dont' want to remove the 5.4 and go back to 5.3.

    Regards,

    Tony

  • Hi Tony,

    I am going to move this to the stellaris forum ... they may be better able to help you as this seems an RTOS issue.   RTOS does not come from the CCS team.

    All the best,

    Lisa