Hello,
I wrote a ton of examples that all run on the Stellaris LaunchPad. All use StellarisWare, there's no direct calls to the device specific files. I'm now evaluating porting these to the new Tiva Launchpad and using TivaWare, but I want the user to be able to download the code to the Stellaris Launchpad too without a problem. Is that true? I'm not using the QEI or USB interfaces.
Thanks,
Derek