HI forum members i have a problem with my PWM signal generation in TMS470. Below is the description of the problem In HET module, PWM Input capture is read through 'capgetsignal' function. While doing so the function returns dutycycle and period as Zero all the time. After adding the variable to watch, the watch values were observed as in screenshots. The watch data is available for both Input and Output. PWM outputs are working fine, the problem is with Input capture. attached screen shot in PDF regards Ram