Hi, it seems that TM4C1231H6PGE OrCad symbol is damaged. Can't import into PADS. Can anyone fix this? Would be useful to provide MentorGraphics format, as well. Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, it seems that TM4C1231H6PGE OrCad symbol is damaged. Can't import into PADS. Can anyone fix this? Would be useful to provide MentorGraphics format, as well. Thanks
Hi,
The most likely issue is that the OrCAD format is newer than the PADS translator. Lagging translators is always an issue with moving from one PCB tool suite to another. The OrCAD files available for download are v16.6, so hopefully Mentor adds support for 16.6 very soon. In the meantime I've attached the TM4C123_ lib saved as v16.2 (thanks Stellaris John). We've confirmed that this format works with PADS 9.3 (and should work with PADS 9.4 and 9.5).
Thank you Jonathan,
The file you provided converted without any problems. (I'm using PADS 9.5). Also, thanks for a quick response.
Rostyslav
BTW, do you provide footprint (land pattern) files as well? The ones for MSP430 are pretty good quality.
Rostyslav
We do not presently provide PCB footprint libraries for TM4C123 series devices, but plan to have them available in a few months.