Other Parts Discussed in Thread: HALCOGEN
Hi~, I'm using LwIP in to ask questions about any problems that have occurred.
Icludes the following topics:
1. Environment
RM48HDK
CCS 5.3.0
HALCoGen 03.05
SafeRTOS
2. Description
I got HALCoGen_EMAC_Driver_and_lwIP_Demonstration-000100.exe(HALCoGen+LwIP Demo for RM48) from website.
<Install Folder>
├──build-rm48 CCSv5 Project for RM48xxx
├──build-tms570 CCSv5 Project for TMS570
├──docs Documents
├──example lwIP Example root
│ └──hdk HDK Port of lwIP example
├──halcogen-rm48 Root folder for HALCoGen generated files for RM48
├──halcogen-tms570 Root folder for HALCoGen generated files for TMS570
└──lwip-1.3.2 Root folder of lwIP files
├──apps Applications root folder
│ └──httpserver_raw_io HTTP Server Application root
│ └──fs File System for HTTP Server
├──doc lwIP Docs folder
├──ports lwIP Port root
│ └──hdk lwIP Port to HDK
└──src lwIP Source folder
LwIP in this demo is standalone system and is set to DHCP. DHCP is running successfully. And then, I have changed NO_SYS(lwipopts.h) to 0 for using lwip under SafeRTOS on RM48HDK. As a result, the following error has occured.
undefined symbol in file
--------- ----------------
sys_arch_mbox_fetch ./lwip-1.3.2/ports/hdk/lwiplib.obj
sys_arch_mbox_tryfetch ./lwip-1.3.2/ports/hdk/lwiplib.obj
sys_arch_sem_wait ./lwip-1.3.2/ports/hdk/lwiplib.obj
sys_arch_timeouts ./lwip-1.3.2/ports/hdk/lwiplib.obj
sys_init ./lwip-1.3.2/ports/hdk/lwiplib.obj
sys_mbox_free ./lwip-1.3.2/ports/hdk/lwiplib.obj
sys_mbox_new ./lwip-1.3.2/ports/hdk/lwiplib.obj
sys_mbox_post ./lwip-1.3.2/ports/hdk/lwiplib.obj
sys_mbox_trypost ./lwip-1.3.2/ports/hdk/lwiplib.obj
sys_sem_free ./lwip-1.3.2/ports/hdk/lwiplib.obj
sys_sem_new ./lwip-1.3.2/ports/hdk/lwiplib.obj
sys_sem_signal ./lwip-1.3.2/ports/hdk/lwiplib.obj
sys_thread_new ./lwip-1.3.2/ports/hdk/lwiplib.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking
----------------------------------------------------------------------------------
These functions are only declared(lwip-1.3.2\src\include\lwip\sys.h) and not the source code(lwip-1.3.2\ports\hdk\sys_arch.c).
What is the way to solve this problem?
Can I get the necessary new sys_arch files?
Please help me~
Thanks.