Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137 Watchdog Timer Expire Reset

Hi,

I am trying to use the RTI Digital Watch Dog Timer in the TMS570LS31x HDK. I read the documentation spna499a. It only mentions that  an NMI or reset is generated

on expiry of the Watch Dog Timer. But it does not give a way to specify which of the above actions is performed. When the watchdog timer is initialized the MCU

simply stops working, without performing any resets. Please provide the necessary information to configure a System Reset in case of Watch Dog Timer expiry.

Regards,

Pritesh

  • We have received your question. We will get back to you as soon as possible.

    Thanks,

    Jay

  • Pritesh,

    The selection between NMI and RESET is done using the RTIWWDRXNCTRL as explain below.

    The DWWD NMI is connected to ESM Group 2 bit 24.

    ESM group2 always generate NMI when the corresponding channel is active.

    If a DWWD NMI is active, the bit 24 of ESMSR2 will be set (Status)

    For the CPU to react on NMI, the F bit is CPSR as to be cleared.
    Out of reset the CPU is IRQ and NMI disable. Once NMI are enable, they cannot be disable anymore by software. Only a CPU Reset will disable NMI.

  • Hi Jean,

    Thank you for the prompt reply. Your answer is built with the assumption of using the Digital Windowed Watchdog(DWWD) Mechanism.

    But what is the control procedure of the timeout expiry of the DWD? Or is there no such concept at all in this case? If so, then the text in the Reference manual should be modified. 

    Regards,

    Pritesh

  • Pritesh,

    I'm not sure I understand your question but I will try to explain with my word the difference between DWD and DWWD.

    Out of reset, the DWD or DWWD is disable. Once it is enable it will stay enable until a device reset.
    The DWD runs out of RTI1 Clock that is used to decrement a 25bits counter. The default value for this down counter is 0x1FFFFFF.
    This default value can be changed via Digital Watchdog Preload Register (RTIDWDPRLD) [offset = 94h]. This register is a 12 bits register.
    The time out will be:

    Time Expitation = (DWDPRLD+1) x 213 / RTICLK1
    where: DWDPRLD = 0...4095

    The preload value has to be set BEFORE the DWD is enable.

    To enable the DWD, Digital Watchdog Control Register (RTIDWDCTRL) [offset = 90h] has to be used.
    Writing 0xA98559DA to RTIDWDCTRL enable the DWD. The DWD will stay enable and will use the RTIDWDPRLD preload value until the next device reset.

    For DWD, at anytime during the down count, the key sequence can be written to DWD to reload the counter with the preload value and avoid RESET or NMI.
    RTI Watchdog Key Register (RTIDWDKEY) [offset = 9Ch] has to be used to write the key sequence.
    A write of E51Ah followed by A35Ch in two separate write operations defines the key sequence and reloads the DWD with the preload value. Writing any other value causes a reset or NMI.

    For DWWD, the key sequence has to be written within a specific time window.
    The DWWD uses the Digital Watchdog (DWD) pre-load register (RTIDWDPRLD) setting to define the end-time of the window.
    The start-time of the window is defined by a window size configuration register Digital Windowed Watchdog Window Size Control (RTIWWDSIZECTRL) [offset = A8h].
    Any attempt to service the watchdog outside this time window, or a failure to service the watchdog in this time window, will cause the watchdog to generate either a reset or a NMI to the CPU.

    All these information are available in the Technical Reference Manual available at: http://www.ti.com/lit/ug/spnu499a/spnu499a.pdf

    Please let me know if I've clarify and answer your question.



  • Hi Jean,

    Thank you once again for your reply. My doubt is something different. 

    How do I set the Reaction of the Digital Watchdog Timer? That is, how do I set the action(either RESET or NMI) after the Timer expires. As far as I saw in the manual,

    there is a section 13.3.33 in SPNA499A which explains this for the DWWD (RTIWWDRXNCTRL register). 

    But in the sections specific to DWD i.e. Sections 13.3.28, 13.3.29, 13.3.30, 13.3.31,13.3.32,  I did not find a description about how to set the reaction on expiry of the DWD.

    Maybe I am missing something? Or the reaction is controlled by the RTIWWDRXNCTRL register for the DWD also?

    Regards,

    Pritesh

  • Pritesh,

    Sorry for the confusion.

    To decide between NMI or RESET for DWD/DWWD you have to use:

    Please let me know if this time I've answer your question.

  • HI Jean,

    Yes, that puts to rest all my doubts. Thank you. The problem was due to the convention of nomenclature of the registers.

    Regards,

    Pritesh