This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TivaWare does not define StellarisWare's HibernateClockSelect(HIBERNATE_CLOCK_SEL_RAW)

I am porting to TivaWare and I am getting compiler errors selecting the hibernate clock.  Is this function call no longer necessary?

For the note on Stellaris where, of the two arguments defined, only one was implemented.  So I can see why this functionality is just now hardwired to the only working option.

If so, this would be a good bullet to add to the porting guide.

  • John,

    I am a little unclear on what you are asking. Do you have a problem, or did you find the solution and are reccomending we document it better? Have you checked out the migration guide (http://www.ti.com/lit/an/spma050a/spma050a.pdf)?

    Regards,

    -Austin

  • I would say yes, both.

    I am asking a question, that I am pretty sure I figured out the answer to and just want a confirmation.

    There is no section on hibernation in the porting guide.  I am suggesting that regardless to the answer above, this function needs to be addressed in the porting guide and it is not.