This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65381 - SEL_VDD3/5

Hi,

there are two different statements about this pin:

datasheet, page 6 and 70:
SEL_VDD3/5 pin open: 3.3V                 SEL_VDD3/5 to ground: 5V

datasheet, page 53 and 63
5V setting (pin SEL_VDD3/5 no-Connect)
3.3V setting(pin SEL_VDD3/5 connected to ground)

Which one is correct?

Best regards,

Andy