Other Parts Discussed in Thread: EK-LM3S811, UNIFLASH, LMFLASHPROGRAMMER, TM4C123GH6PGE
Customer is at the end of the board integration that base on Stalaris LM4F232 chip. would like to use a LM flash programmer s.w. for burning the firmware to my board. I'm considering the following option:
1. Use JTAG interface - Is there a board that use as an interface between my board with J-tag interface and PC? Can I use the LM4F232HQD evaluation board for this purpose?
2. Use the UART interface - does the f.w. download can be done via UART 0 only? Is there a need for s.w. configuration of the BOOT loader?
Is there someone that I can meet with in order to consult with?