hi,
i am not actually where the problem is i used the correct slave address also that is 0xD0.
void RTC_read()
{
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, SLAVE_ADDRESS, true); // Read Start
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_START);
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
timeformat[0]=I2CMasterDataGet(I2C0_MASTER_BASE); //Receive zero byte
ROM_UARTCharPutNonBlocking(UART7_BASE, timeformat[0]);
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_CONT);
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
timeformat[1]=I2CMasterDataGet(I2C0_MASTER_BASE); //Receive 1stbyte
ROM_UARTCharPutNonBlocking(UART7_BASE, timeformat[1]);
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_CONT);
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
timeformat[2]=I2CMasterDataGet(I2C0_MASTER_BASE); //Receive 2nd byte
ROM_UARTCharPutNonBlocking(UART7_BASE, timeformat[2]);
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
timeformat[3]=I2CMasterDataGet(I2C0_MASTER_BASE); //Receive 3rd byte
ROM_UARTCharPutNonBlocking(UART7_BASE, timeformat[3]);
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
}
//*****************************************************************************
//
// Configure the I2C0 master and slave and connect them using loopback mode.
//
//*****************************************************************************
int
main(void)
{
//unsigned long ulDataTx;
unsigned int i;
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_8MHZ);
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
GPIOPinTypePWM(GPIO_PORTB_BASE, GPIO_PIN_2);
//HWREG(I2C0_MASTER_BASE + I2C_O_MCR) |= 0x01;
IntEnable(INT_I2C0);
I2CSlaveIntEnableEx(I2C0_SLAVE_BASE, I2C_SLAVE_INT_DATA);
I2CMasterInitExpClk(I2C0_MASTER_BASE, SysCtlClockGet(), false);
I2CSlaveEnable(I2C0_SLAVE_BASE);
//I2CSlaveInit(I2C0_SLAVE_BASE, SLAVE_ADDRESS);
//I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, SLAVE_ADDRESS, false);
InitConsole(); //uart init
IntMasterEnable();
// Display the example setup on the console.
//
UARTSend((unsigned char*)"I2C Slave Interrupt Example ->",40);
delay();
UARTSend((unsigned char*)"\n Module = I2C0",20);
delay();
UARTSend((unsigned char*)"\n Mode = Receive interrupt on the Slave module",50);
delay();
UARTSend((unsigned char*)"\n Rate = 100kbps\n\n",35);
//ulDataTx = 'S';
UARTSend((unsigned char*)"Transferring from: Master -> Slave\n",50);
delay();
rtc_write();
while(1)
{
RTC_read();
}
}
void rtc_write()
{
I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, SLAVE_ADDRESS, false); // Write
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
I2CMasterDataPut(I2C0_MASTER_BASE, 0x00); // Address Offset
// Initiate send of character from Master to Slave
I2CMasterControl(I2C0_MASTER_BASE,I2C_MASTER_CMD_BURST_SEND_START); //0x003
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
I2CMasterDataPut(I2C0_MASTER_BASE, 0x01); // Seconds
// Initiate send of character from Master to Slave
I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
I2CMasterDataPut(I2C0_MASTER_BASE, 0x02); // Minutes
// Initiate send of character from Master to Slave
I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
I2CMasterDataPut(I2C0_MASTER_BASE, 0x09); // hours
// Initiate send of character from Master to Slave
I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_FINISH);
while(I2CMasterBusy(I2C0_MASTER_BASE))
{
}
}