Hello,
I am currently designing a board with a TMS5703137BZWTQQ1 and have to look at each pin for all my desired functions.
For these 4 pin functions, two ball grid pins are assigned (document SPNS162A –APRIL 2012–REVISED NOVEMBER 2012)
HET1_21: H4 J3
HET1_27: A9 B2
HET1_29: A3 C3
GIOB_2: F2 V10
Is this some kind of error or is this correct? How can one have the same pin function (like GIOB_2) on two different pins? E.g. how can one read one GIO B2 input from two different pins?
Would be great if someone from TI could clarify this.
Thanks,
Tom