This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error connecting to target

Hello, 

I am running a laptop with Ubuntu 12.04LTS on it using CCS5.4 to try and communicate with a Stellaris LM4F120 Board.  I have a project that that builds without error, but when I go to debug it I get this error:  CORTEX_M4_0: Error connecting to the target

I have double checked the plugs on the mini-USB and the USB on the laptop.  When the board is connected to the laptop the port is enumerated as /dev/ttyACM0. Which is the same port enumerated on another laptop.

We don't have any problems connecting to another laptop with the same configuration.  Both laptops are Lenovo though one is a slightly different model. It shouldnt make a difference.