This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AN01272 Source

Another question on evaluation kit EKI-LM4F232. 

Included in the documentation is application note AN01272.  It doesn't do anything other than reference source code which does not appear to be included and which all references appear to be dead.

Where can I get the source?  Maybe I've just missed the reference?

Robert

  • Hi Robert,

    AN01272 is the IEC 60730 app note correct? 

    That material and the referenced libraries are no longer available and there are no current options for IEC60730 with LM4F/TM4C.  There are other options though, such as MSP430 and C2000.

    http://www.ti.com/ww/en/functional_safety/safeti/SafeTI-60730.html

    I hope this answers your question.

  • That's the one.  Since the app-note was present on the disk with the evaluation kit, I rather expected the software would be available giving a good start on adding self tests.

     

    It would be a good idea to remove that appnote from the disk or mention that it doesn't apply to the products it's included with.

     

    Robert