This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTSC support for RM48

Hello,

I would like to use the Real-Time Software Component (RTSC).

I'm using the development board TMDXRM48HDK equipped with the ARM RM48.

When I create a RTSC project it seems that RM48 is not supported.

If I use as target: ti.targets.arm.elf.R4F, there is no RM48 platform available.

Then I use the generic platform, but with no success (error: Parameter 'deviceName' must be specified for 'xdc.platform.generic' platform)

Thanks.