Other Parts Discussed in Thread: RM48L952, HALCOGEN
Hi, section 5.2.1 of the RM48L952 data sheet says: "Total Sample/Hold/Convert time: 600ns Typical Minimum at 30MHz ADCLK". Does this mean it is possible to achieve ~1.6MSPS? Also, HalCoGen seems to suggest that the ADC RAM is 64 words long... does this mean you can do up to 64 samples before reading out the results? Finally, do you think it would be possible to achieve ~625kSMS continously at 10 bit resolution? We are particularly interested in the phase of the signal so timing, especially between start new transfer groups, is important. Note also that I'm already pushing ~75Mbit/s through the DMA (SPI).
Thanks,
Jack