Other Parts Discussed in Thread: UNIFLASH, TMS570LS3137
Dear all,
if I use UniFlash ( Version: 2.1.0.00009 ) I am not able to connect with the target (TMS570LS3137 on the HDK) via the debugger Spectrum Digital XDS510usb plus.
I get following error message - complete console record:
Begin Launching session operation...
Operation Launching session returned.
Loaded target configuration from: C:\Users\JIRI~1.JAN\AppData\Local\.TI\2086677247\0\0/temptargetconfiguration.ccxml
Settings purged.
Erasing flash sectors on Core 0 < Spectrum Digital XDS510USB Emulator/CortexR4 > ...
FATAL >> IcePick: Error connecting to the target: Error 0x80000244/-2131 Fatal Error during: Register, Initialization, OCS, Cannot access register at 0x00000000
BooleanEventCallback error!!! false
If I used the Code Composer v5 the target is connected properly and all the operations can be done (erase, flash, verify,...). But for further purpose I cannot use CCS, so UniFlash is the option for me.
At the best I would like to use nowFlash v3.42 but that also crashes with an error (id = 199).
Do you have any idea what is going wrong?
Thanks a lot in advance,
Best regards, Jiri