Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SSI0 slave clock speed

Other Parts Discussed in Thread: TM4C1231H6PGE

Hallo,

I have TM4C1231H6PGE and tivaware 1.0.

I use SPI0 as slave. Master set SPI clock to 19200. I wonder what value set in

ROM_SSIConfigSetExpClk(SSI0_BASE, 24576000UL, SSI_FRF_MOTO_MODE_0, SSI_MODE_SLAVE, 192000, 8);

Keep in mind that core master clock is 24.576 MHz (PLL is bypassed).

I have tried 3 different values: 19.2 KHz, 192 KHz and 4.096 MHz.


when I set 192KHz the receive interrupt is triggered after about 165 us from last sclk edge (note that 165 us is about 32 times clock period @192KHz):

despite this, only one character is poped from FIFO, as if there were only one.

If I set 19.2KHz or 4.096MHz the interrupt is triggered after first character and no other interrupt are triggered:

Where am I worng? What are the clock speed limits for my configuration? How to calculate them?

I have attached the slice of code I use.

best regards