Hi Friend, after a long effort I discovered that my hardware was with problem, that now has solved .
After initial test I verified that when I try write in SD CARD my code, return error.
The error showed by FATFS is FR_INVALID_OBJECT
I Verified this error on FATFS site and the message meaning :
FR_INVALID_OBJECT : The file/directory object is invalid or a null pointer is given.
My code is paste below, someone can help me understand why this error happen and what I need to do to solve this. Thanks too much and have a good day .
//*****************************************************************************
//
// sd_card.c - Example program for reading files from an SD card.
//
// Copyright (c) 2011-2012 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 9453 of the EK-LM4F232 Firmware Package.
//
//*****************************************************************************
#include <string.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "utils/cmdline.h"
#include "utils/uartstdio.h"
#include "third_party/fatfs/src/ff.h"
#include "third_party/fatfs/src/diskio.h"
#include "third_party/fatfs/port/mmc-ek-lm4f232h5qd.h"
#define GPIO_PA0_U0RX 0x00000001
#define GPIO_PA1_U0TX 0x00000401
#define GPIO_PA2_SSI0CLK 0x00000802
#define GPIO_PA3_SSI0FSS 0x00000C02
#define GPIO_PA4_SSI0RX 0x00001002
#define GPIO_PA5_SSI0TX 0x00001402
static FIL Fil;
//#define NUM_SSI_DATA 3
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>SD card using FAT file system (sd_card)</h1>
//!
//! This example application demonstrates reading a file system from an SD
//! card. It makes use of FatFs, a FAT file system driver. It provides a
//! simple command console via a serial port for issuing commands to view and
//! navigate the file system on the SD card.
//!
//! The first UART, which is connected to the USB debug virtual serial port on
//! the evaluation board, is configured for 115,200 bits per second, and 8-N-1
//! mode. When the program is started a message will be printed to the
//! terminal. Type ``help'' for command help.
//!
//! For additional details about FatFs, see the following site:
//! http://elm-chan.org/fsw/ff/00index_e.html
//
//*****************************************************************************
//*****************************************************************************
//
// Defines the size of the buffers that hold the path, or temporary data from
// the SD card. There are two buffers allocated of this size. The buffer size
// must be large enough to hold the longest expected full path name, including
// the file name, and a trailing null character.
//
//*****************************************************************************
#define PATH_BUF_SIZE 80
//*****************************************************************************
//
// Defines the size of the buffer that holds the command line.
//
//*****************************************************************************
#define CMD_BUF_SIZE 64
//*****************************************************************************
//
// The following are data structures used by FatFs.
//
//*****************************************************************************
static FATFS g_sFatFs;
//*****************************************************************************
//
// A structure that holds a mapping between an FRESULT numerical code, and a
// string representation. FRESULT codes are returned from the FatFs FAT file
// system driver.
//
//*****************************************************************************
typedef struct
{
FRESULT fresult;
char *pcResultStr;
}
tFresultString;
//*****************************************************************************
//
// A macro to make it easy to add result codes to the table.
//
//*****************************************************************************
#define FRESULT_ENTRY(f) { (f), (#f) }
//*****************************************************************************
//
// A table that holds a mapping between the numerical FRESULT code and it's
// name as a string. This is used for looking up error codes for printing to
// the console.
//
//*****************************************************************************
tFresultString g_sFresultStrings[] =
{
FRESULT_ENTRY(FR_OK),
FRESULT_ENTRY(FR_NOT_READY),
FRESULT_ENTRY(FR_NO_FILE),
FRESULT_ENTRY(FR_NO_PATH),
FRESULT_ENTRY(FR_INVALID_NAME),
FRESULT_ENTRY(FR_INVALID_DRIVE),
FRESULT_ENTRY(FR_DENIED),
FRESULT_ENTRY(FR_EXIST),
FRESULT_ENTRY(FR_RW_ERROR),
FRESULT_ENTRY(FR_WRITE_PROTECTED),
FRESULT_ENTRY(FR_NOT_ENABLED),
FRESULT_ENTRY(FR_NO_FILESYSTEM),
FRESULT_ENTRY(FR_INVALID_OBJECT),
FRESULT_ENTRY(FR_MKFS_ABORTED)
};
//*****************************************************************************
//
// A macro that holds the number of result codes.
//
//*****************************************************************************
#define NUM_FRESULT_CODES (sizeof(g_sFresultStrings) / sizeof(tFresultString))
//*****************************************************************************
//*****************************************************************************
//
// This function returns a string representation of an error code that was
// returned from a function call to FatFs. It can be used for printing human
// readable error messages.
//
//*****************************************************************************
const char *
StringFromFresult(FRESULT fresult)
{
unsigned int uIdx;
//
// Enter a loop to search the error code table for a matching error code.
//
for(uIdx = 0; uIdx < NUM_FRESULT_CODES; uIdx++)
{
//
// If a match is found, then return the string name of the error code.
//
if(g_sFresultStrings[uIdx].fresult == fresult)
{
return(g_sFresultStrings[uIdx].pcResultStr);
}
}
//
// At this point no matching code was found, so return a string indicating
// an unknown error.
//
return("UNKNOWN ERROR CODE");
}
//*****************************************************************************
//
// This is the handler for this SysTick interrupt. FatFs requires a timer tick
// every 10 ms for internal timing purposes.
//
//*****************************************************************************
void
SysTickHandler(void)
{
//
// Call the FatFs tick timer.
//
disk_timerproc();
//UARTprintf("\n\tick");
}
//*****************************************************************************
//
// This function implements the "ls" command. It opens the current directory
// and enumerates through the contents, and prints a line for each item it
// finds. It shows details such as file attributes, time and date, and the
// file size, along with the name. It shows a summary of file sizes at the end
// along with free space.
//
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, unsigned long ulLine)
{
}
#endif
//*****************************************************************************
//
// The program main function. It performs initialization, then runs a command
// processing loop to read commands from the console.
//
//*****************************************************************************
int
main(void)
{
FRESULT fresult;
static DIR g_sDirObject;
static FILINFO g_sFileInfo;
unsigned long ulTotalSize;
FATFS *pFatFs;
unsigned int bw;
ulTotalSize = 0;
//
// Enable lazy stacking for interrupt handlers. This allows floating-point
// instructions to be used within interrupt handlers, but at the expense of
// extra stack usage.
//
ROM_FPULazyStackingEnable();
//
// Set the system clock to run at 50MHz from the PLL.
//
// ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
// SYSCTL_XTAL_16MHZ);
ROM_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
//
// Enable the peripherals used by this example.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//_______________________________________________
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
//_______________________________________________
//
// Configure SysTick for a 100Hz interrupt. The FatFs driver wants a 10 ms
// tick.
//
ROM_SysTickPeriodSet(ROM_SysCtlClockGet() / 100);
ROM_SysTickEnable();
ROM_SysTickIntEnable();
//
// Enable Interrupts
//
ROM_IntMasterEnable();
//
// Set GPIO A0 and A1 as UART.
//
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Initialize the UART as a console for text I/O.
//
UARTStdioInit(0);
//
// Print hello message to user.
//
UARTprintf(" uSD FIRMWARE V.10072013\n");
UARTprintf(" Iniciando montagem do volume \n");
//
// Mount the file system, using logical disk 0.
//
UARTprintf(" Inicializando SDCARD \n");
while(disk_initialize(0));
UARTprintf(" SDCARD Iniciado com sucesso \n");
fresult = f_mount(0, &g_sFatFs);
if(fresult != FR_OK)
{
UARTprintf("f_mount error: %s\n", StringFromFresult(fresult));
return(1);
}
else
{
UARTprintf("FR_OK \n");
}
fresult = f_getfree("/", &ulTotalSize, &pFatFs);
UARTprintf(", %10uK bytes free\n", ulTotalSize * pFatFs->sects_clust / 2);
fresult = f_open(&Fil, "message.TXT", FA_WRITE | FA_CREATE_NEW);
if (fresult != FR_OK )
{
UARTprintf(" ERRO \n");
}
else
{
UARTprintf(" CARTÃO ABERTO \n");
}
fresult = f_write(&Fil, "teste escrita realizado com sucesso \r\n", 35 ,&bw);
if (fresult != FR_OK )
{
UARTprintf(" WRITE ERROR \n");
UARTprintf("Erro de escrita : %s\n", StringFromFresult(fresult));
}
else
{
UARTprintf(" escrita realizada com sucesso \n");
}
fresult = f_close(&Fil);
if(fresult != FR_OK)
{
UARTprintf("Falha ao finalizar o SDCARD ", StringFromFresult(fresult));
return(1);
}
else
{
UARTprintf("Cartão Finalizado \n");
}
}