Other Parts Discussed in Thread: UNIFLASH, TMS470MF06607
Hi,
I am using a XDS510 emulator and a TMS470.
What I did do
I started to to download the program via CCS to the board. When the flashing process has started I made the mistake (apparently) to cancel the flashing but at the same power off the board!
Since then I get the following message:
Error connecting to the target:
Error 0xC0002240/-5008
Error during: Initialization, OCS, Control,
Unknown Error
We have other identical TMS470 boards and the XDS510 is functioning because I am able to flash those so the emulator is OK.
It seems something happened inside the TMS470 when I turned off the power during flashing.
I have tried nowFlash and UniFlash and tried to erase the flash but they return about the same error messages.
Any ideas?
Best regards,
Lars von Wachenfeldt