Other Parts Discussed in Thread: TM4C123GH6PZ
Hello,
I am working on a project where we need to upgrade firmware on the device in the field , i understand that this may be achieved using the bootloader of Tivaware but i have the following questions
I am using TM4C123GH6PZ processor
1 >> Can i upgrade the firmware using USB stick / thumb drive ?
2 >> Can the upgrade be done on windows 7 using GUI or any other methods
3>> If i want to lock the flash what options are available (hardware / firmware)
Regards
Abhay