Hi, I have got an error in CCS 5.2.1 during debugging: CORTEX M4_0: Frequency is out of range. I have reinstalled ICDI drivers (i have tried drivers from CCS directory, and from ti site also), then tried to unlock target with the LM flash programmer, nothing to help. I see Stellaris ICDI and Virtual COM port in the device manager, but I can't connect to it with CCS or LM Flash programmer. When I trying to connect via LM flash programmer, the error appers "target is not connected".
Problem appeared when I finished lab5 (ADC, rom functions, volatile variables) and tried to debug lab6. Now, the green color of RGB led blinks twice when I power up board, then go out.
What should I do?