Other Parts Discussed in Thread: HALCOGEN
Hi,
I want to develop Ethernet communication between PC and HDK board where i want duplex communication betn the two. I need info abt d following thing,
1. From where should i start?? (I found Lwip pdf. is it where i should start?)
2. Which version of CCS i need?? (only 5.4 where Halcogen support is available or any lower version is also k. Also Is Win. 7 is OK for this purpose?? or i need some different O.S.)
3.Where can i get any sample example wrt ehternet implementation?
4. Is it necessary to use Halcogen or i can also develop application without it?
5. What if i don't want to use web browser? is there any other way (lwip with different applicaiton layer used)
Kindly provide me with the above info.
Thanks in advance.
Regards,
Manmesha.