This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM46 - TSCTR running at which frequency?



Hi there,

I'm using the eCAP module of the RM46 controller.

User manual page 236 (4.5.9) says:
"The VCLK4 domain is used as the clock for the eCAPx modules"

User manual page 800 (20.4.4) says:
"This counter provides the time-base for event captures, and is clocked via the system clock"

As far as I know, these ( system clock(also named HCLK) and VLCK4) are two different clocks.
So, which statement is correct?

Best regards,

Andy