Other Parts Discussed in Thread: TM4C123GH6PM
Hi,
We need some clarifications about the TIVA C ADC reference.
The "System Design Guidelines for Tiva™ C Series" mentiones as below about the internal reference
"Tiva C Series TM4C microcontrollers offer greater ADC precision and require an external reference
voltage. The TM4C circuit should provide a precision voltage source to either the VREF+ or VDDA pin.
The designer should determine whether the internal reference has sufficient accuracy or if an external
reference is needed"
1.Just wanted to clarify that,there is no internal reference for ADC in TIVA C?
In case of devices like "TM4C123GH6PM" which do not have the "VREFA+ and VREFA-" reference input,
I think VDDA and GNDA is the only option for voltage reference.
2.But the VDDA is also the supply for all of the analog circuitry on the device(including the clock circuitry)
which may be affected due to internal voltage drop, so in order to get the precise ADC measurements
what are necessary things have to be considered with VDDA(as the voltage reference)?
Best Regards.
Prad.