Other Parts Discussed in Thread: HALCOGEN
Hi,
I have several questions about HALCoGen 03.05.02 .
Q1: I just want to use few pins of MibSPI as GIO. Do I have to enable the "MibSPI driver" in "RM48L952PGE--->Driver Enable" of HALCoGen 03.05.02 ?
if a driver is disable in "RM48L952PGE--->Driver Enable" of HALCoGen 03.05.02 , It's code (like it's *.h and *c files) will not be compiled and linked, is it correct?
Q2: When I change the project and generate the code in HALCoGen 03.05.02, Sometimes the CCS5.4 which share the project with HALCoGen 03.05.02 show me an update prompt, Sometimes it does no show the prompt. why?
Thanks,
Chuan