This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

stellaris launchpad I2C0 periperal with eeprom At24c04

hai this is my program in t his i am given data to eeprom from i2c master is Indata[6]= {0x00,0x03,0x05,0x07,0x09,0x11}; but i read data from eeprom is 37,38,39,0B,0C,0D what is the problem in this code.

#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_i2c.h"
#include "driverlib/i2c.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"

#define GPIO_PB2_I2C0SCL        0x00010803
#define GPIO_PB3_I2C0SDA        0x00010C03
#define SLAVE_ADDRESS 0x54
int i;
unsigned char byte_rcv;
unsigned char Outdata[6];

void main(void)
{
    unsigned short reg_address=0x000;


      unsigned char Indata[6]= {0x00,0x03,0x05,0x07,0x09,0x11};
      unsigned char Outdata[6]= {0x00,0x00,0x00,0x00,0x00,0x00};
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |SYSCTL_XTAL_16MHZ);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);


    GPIOPinConfigure(GPIO_PB2_I2C0SCL);
    GPIOPinConfigure(GPIO_PB3_I2C0SDA);
    GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2 );
    GPIOPinTypeI2C(GPIO_PORTB_BASE,  GPIO_PIN_3);

    I2CMasterInitExpClk(I2C0_MASTER_BASE, SysCtlClockGet(), false);
    I2CMasterEnable(I2C0_MASTER_BASE);
    I2CMasterIntDisable(I2C0_MASTER_BASE);
    I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, SLAVE_ADDRESS, false);
    I2CMasterDataPut(I2C0_MASTER_BASE,reg_address);
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_START);
    while(I2CMasterBusy(I2C0_MASTER_BASE));
    for(i=0; i < 6; i++)
    {
    I2CMasterDataPut(I2C0_MASTER_BASE,Indata[i]);
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
    while(I2CMasterBusy(I2C0_MASTER_BASE));
    }
    I2CMasterDataPut(I2C0_MASTER_BASE,Indata[i]);
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_SEND_FINISH);
    while(I2CMasterBusy(I2C0_MASTER_BASE));
     SysCtlDelay(SysCtlClockGet() / 500);
    I2CMasterIntEnable(I2C0_MASTER_BASE);
    I2CMasterIntDisable(I2C0_MASTER_BASE);
    I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, SLAVE_ADDRESS, false);
    I2CMasterDataPut(I2C0_MASTER_BASE,reg_address);
    while(I2CMasterBusy(I2C0_MASTER_BASE));
    I2CMasterSlaveAddrSet(I2C0_MASTER_BASE, SLAVE_ADDRESS, true);
     i=0;
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_START);
    while(I2CMasterBusy(I2C0_MASTER_BASE));
    byte_rcv = I2CMasterDataGet(I2C0_MASTER_BASE);
    Outdata[0] = byte_rcv;
    for(i=1; i < 6; i++)
            {
        I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_CONT);
                while(I2CMasterBusy(I2C0_MASTER_BASE));
        byte_rcv = I2CMasterDataGet(I2C0_MASTER_BASE);
        Outdata[i] = byte_rcv;
            }
    I2CMasterControl(I2C0_MASTER_BASE, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
        while(I2CMasterBusy(I2C0_MASTER_BASE));
        byte_rcv = I2CMasterDataGet(I2C0_MASTER_BASE);
        Outdata [i] = byte_rcv;
    I2CMasterIntEnable(I2C0_MASTER_BASE);
    }