Hello, I have a question regarding the Tiva C Launch Pad Eval Kit schematic. On page 3 you have PD6, PF1, and PF2 connected to I/O pins. You then have ports PA2, PA3, and PA4 connected to the DEBUG/VCOM Bus that is the JTAG interface to the main MCU. My question is what are the actual pin needed to connect to the MAIN MCU to support the ICDI? What are ports PD6, PF1, and PF2 used for since they are named the same as PA2-PA4? Any insight would be greatly appreciated. Thank you,
Rob