Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CRC algorithm for 20216 CRC module

Other Parts Discussed in Thread: TMS570LS20216, HALCOGEN, TMS570LS3137

Hi,

I am working on TMS570LS20216. I am working on generating RAM CRC and CPU registers CRC using CRC module of TMS570. I am using FULL CPU MODE.

Can I use CRC modules generated by Halcogen using tms570_hdk as Halcogen for 20216 does not geneate CRC module. Also can CRC files be used as is for TMS570LS20216?

Where can I get the CRC algorithm for 20216 CRC module? I should pre calcuate CRC using the same algorithm, to verify PSA register calculated CRC with pre calculated CRC .

Thank you for your support.

Regards,

Chitra

  • I split the thread because the old thread has been closed.

    Yes, they have the same CRC module.

    The CRC algorithm can be found in the TRM  22.3.3 PSA Signature Register.

    We have two CRC signature registers, high and low. I can provide you the example/code to pre calcuate CRC by 32-bit write, that is, write the CRC signature high and low register seperately.

    I am not very clear about whether a 64-bit write works. Do both DMA and CPU 64-bit write work? I will check and give you feedback in a few days. 

    Regards,

    Haixiao

  • Hi,

    Thank you for splitting the thread. Actually I am not well versed with community pages. I could not conclude how to create new thread?

    Actually I am trying to use this CRC algorithm/function as an API. Can I use it like that? I am trying to pass the data to structure "crcModConfig_t" in the field "src_data_pat". Then I can calculate CRC of that using PSA registers.

    Let me know if I can do that.

    Regards,

    Chitra

  • Click the "New Post" button to post something new:

    I will give you an example to calculate the CRC using hardware and software.

    Haixiao

  • Here is an example project of calculating CRC.

    2744.CRC_Example.zip

    I run this software using the USB stick. And it will output the result to the PC end Hyperterminal (19.2k baudrate, no parity, one stop bit.)

    There are six important functions in this example:

    1) CPU write to the CRC module Hardware (32bit write) to calculate the CRC of a sector of numbers in CRC_Pattern.c.

    This function (crcSignGen) is generated by HalCoGen (CRC.h, CRC.c), I copy the TMS570LS3137 CRC files here.

    2) Using the CPU software (SoftCrcCal_32) to emulate the CRC calculation of the same data sector (32bit write) 

    This function is located in soft_CRC.c.

    3) DMA write (dmaConfigCtrlPacket_32 and others) to the CRC module Hardware (32bit write) to calculate the same data sector

    These functions are located in sys_main.c and sys_dma.c. I did not merge them into one function.

    4) CPU write to the CRC module Hardware (64bit write) to calculate the CRC of a sector of numbers in CRC_Pattern.c.

    This function (_crcSignGen_64) is located at CRC_64.asm. I have to write in asm to ensure it is a 64 bit access, remove the impact of compilers.

    5) Using the CPU software (SoftCrcCal_64) to emulate the CRC calculation of the same data sector (64bit write) 

    This function is located in soft_CRC.c.

    6) DMA write (dmaConfigCtrlPacket_64 and others) to the CRC module Hardware (64bit write) to calculate the same data sector

    These functions are located in sys_main.c and sys_dma.c. I did not merge them into one function.

    CRC is a tricky module in this device, 32 bit write and 64 bit write generate different result for the same group of data.

    CRC module has three mode, full CPU, semi and auto. The last two mode use DMA transfer. In the example project, I did not demo the usage of sem and auto mode. You can integrate it by yourself. For example, in auto mode, you only get a interrupt once CRC mismatch occurs.

    Regards,

    Haixiao

  • Hi,

    Thank you for an example. I shall work on this in a day's time and get back to you.

    Can I use these function for application CRC or some other data CRC? I read a post which states that CRC module can be used only for calculating CPU/FPU register CRC.

    Thank you for your support

    Regards,

    Chitra

  • Yes, what is CRC doing:

    The master (CPU or DMA) write some data (dont care where it comes from) to the CRC signature register. Then the CRC module generate the CRC signature based on the data written and the initial signature value.

    The previous post is done in compiler 5.1.1A, which is not published yet.
    Here I transfer it into compiler version 4.9.6.8030.CRC_Example.zip

    Regards,

    Haixiao

  • Hi,

    Logically it is correct but since I had read som post about CRC I just thought of confirming.

    Thank you for example wiht correct compiler. I will work on it today.

    For some reason i dont see New Post button on the my page. might be some firewall issue.

    Regards,

    Chitra

  • Hi,

    I have few questions related to the example as my development board got damaged and i am unable to debug my application.

    1) Why do we need CRC using DMA because I am using FULL CPU Mode for the computation? Is it mandatory?

    2) Why do I need SCI_Init function becasue it works fine without this function call as well

    3) What I understand from the example is in case hardware and software crc matches then we can conclude that CRC matches right? I am asking you this becasue I did not find the comparison in the example or is there any other way of comparing and concluding

    4) In the main function from file sys_main.c, do I need to calculate CRC using both 32 (CRCSignLo_hard_32)and 64 (CRCSignLo_hard_64)bits and then compare the results? or if my data is 32 bit Ican use only 32 bit CRC functions and leave rest of them say use ""SoftCrcCal_32" and don't use "SoftCrcCal_64".

    5) In case my data is 32 bit and I am using FULL CPU MODE, I can end my main function after calling "SoftCrcCal_32" in the sys_main.c file

    Regards

    Chitra

  • Chitra Sapre said:

    Hi,

    I have few questions related to the example as my development board got damaged and i am unable to debug my application.

    1) Why do we need CRC using DMA because I am using FULL CPU Mode for the computation? Is it mandatory?

    HW: This is a generic example showing the capabilities of the device. Choose CPU or DMA, whatever you like.

    2) Why do I need SCI_Init function becasue it works fine without this function call as well

    HW: As an example, I output the calculated CRC to the Hyperterminal so that I knew whether the result is correct or wrong. You don't need that in your application.

    3) What I understand from the example is in case hardware and software crc matches then we can conclude that CRC matches right? I am asking you this becasue I did not find the comparison in the example or is there any other way of comparing and concluding

    HW: I output them to the hyperterminal and compare them there. In your application, for the software crc (golden value), you can calculate with you PC or use MCU, and then compare the hardware CRC against this golden value. In the auto mode, you can save the golden value into one CRC registers and the CRC module will trigger an interrupt once the hardware CRC does not match the golden value.

    4) In the main function from file sys_main.c, do I need to calculate CRC using both 32 (CRCSignLo_hard_32)and 64 (CRCSignLo_hard_64)bits and then compare the results? or if my data is 32 bit Ican use only 32 bit CRC functions and leave rest of them say use ""SoftCrcCal_32" and don't use "SoftCrcCal_64".

    HW: No. You only need to calculate one of them. I show you all the calculation because I want to remind you that, 32 bit access and 64 bit access generate different CRC value.

    5) In case my data is 32 bit and I am using FULL CPU MODE, I can end my main function after calling "SoftCrcCal_32" in the sys_main.c file

    HW: SoftCrcCal_32 show you how to calculate the CRC using software, for example, you can port this function to visual C++ and calculate there. With our device, it can is calculated by the hardware CRC module (saves a lot of CPU load).

    Regards

    Chitra

  • Hi,

    Thank you for clarification. My CRC is working fine now.

    I am unable to debug since my assemly routine is throwing error. Error is some where in Halcogen generated asm functions. Error is very simple "Cannot redefine existing opcode 'AND' with .define" but I am unable to locate it. Any suggestions?

     

    Code is pasted for the reference:

    -------------------------------------------------------------------------------------------------------------------------

        .text
        .arm

     .cdecls C,NOLIST
     %{
        #include "ARM/CSA_Defs.inc"
        #include "BT_Startup.h"
     %}
     .include "BT_C_Structure_Offsets.inc"
        .page

    ;-------------------------------------------------------------------------------
    ; Initialize CPU Registers

        .def     _coreInitRegisters_
        .asmfunc

    _coreInitRegisters_

            mov   r0,         lr
            mov   r1,         #0x03D0
            mov   r2,         #0x0000
            mov   r3,         #0x0000
            mov   r4,         #0x0000
            mov   r5,         #0x0000
            mov   r6,         #0x0000
            mov   r7,         #0x0000
            mov   r8,         #0x0000
            mov   r9,         #0x0000
            mov   r10,        #0x0000
            mov   r11,        #0x0000
            mov   r12,        #0x0000
            orr   r13,        r1,     #0x0001
            msr   cpsr_cxsf,  r13
            msr   spsr_cxsf,  r13
            mov   lr,         r0
            mov   r8,         #0x0000
            mov   r9,         #0x0000
            mov   r10,        #0x0000
            mov   r11,        #0x0000
            mov   r12,        #0x0000
            orr   r13,        r1,     #0x0002
            msr   cpsr_c,     r13
            msr   spsr_cxsf,  r13
            mov   lr,         r0
            orr   r13,        r1,     #0x0007
            msr   cpsr_c,     r13
            msr   spsr_cxsf,  r13
            mov   lr,         r0
            orr   r13,        r1,     #0x000B
            msr   cpsr_c,     r13
            msr   spsr_cxsf,  r13
            mov   lr,         r0
            orr   r13,        r1,     #0x0003
            msr   cpsr_c,     r13
            msr   spsr_cxsf,  r13

            fmdrr d0,         r1,     r1
            fmdrr d1,         r1,     r1
            fmdrr d2,         r1,     r1
            fmdrr d3,         r1,     r1
            fmdrr d4,         r1,     r1
            fmdrr d5,         r1,     r1
            fmdrr d6,         r1,     r1
            fmdrr d7,         r1,     r1
            fmdrr d8,         r1,     r1
            fmdrr d9,         r1,     r1
            fmdrr d10,        r1,     r1
            fmdrr d11,        r1,     r1
            fmdrr d12,        r1,     r1
            fmdrr d13,        r1,     r1
            fmdrr d14,        r1,     r1
            fmdrr d15,        r1,     r1
            bl    next1
    next1
            bl    next2
    next2
            bl    next3
    next3
            bl    next4
    next4
            bx    r0

        .endasmfunc

    ;-------------------------------------------------------------------------------
        .def     _coreEnableVfp_
        .asmfunc

    _coreEnableVfp_

            mrc   p15,     #0x00,      r0,       c1, c0, #0x02
            orr   r0,      r0,         #0xF00000
            mcr   p15,     #0x00,      r0,       c1, c0, #0x02
            mov   r0,      #0x40000000
            fmxr  fpexc,   r0
            bx    lr

        .endasmfunc

    ;_coreEnableVfp_
    ;
     ;       mrc   p15,     #0x00,      r0,       c1, c0, #0x02
      ;      orr   r0,      r0,         #0xF00000
       ;     mcr   p15,     #0x00,      r0,       c1, c0, #0x02
        ;    mcr   p15,     #0x00,      r0,       c0, c0, #0x02
         ;   mov   r0,      #0x40000000
          ;  fmxr  fpexc,   r0
           ; bx    lr

       ; .endasmfunc

    ;-------------------------------------------------------------------------------
    ; Enable Offset via Vic controller

        .def     _coreEnableIrqVicOffset_
        .asmfunc

    _coreEnableIrqVicOffset_

            mrc   p15, #0, r0,         c1, c0,  #0
            orr   r0,  r0,    #0x01000000
            mcr   p15, #0, r0,         c1, c0,  #0
            bx    lr

        .endasmfunc

    ;-------------------------------------------------------------------------------
    ; Enable core RAM ECC

        .def _coreEnableRamEcc_
        .asmfunc

    _coreEnableRamEcc_

        ; Enabling reading writing to Secondary Auxiliary Registers

        MRC P15,    #0,     R1,     C9,     C12,    #0
        ORR R1,     R1,     #0x00000010
        MCR P15,    #0,     R1,     C9,     C12,    #0

        ; Enable parity checking DOTCM

        ORR R1,     R1,     #0x1 <<26
        DMB
        MCR P15,    #0,     R1,     C1,     C0,     #1
        ISB

        ; Enable parity checking D1TCM

        MRC P15,    #0,     R1,     C1,     C0,     #1
        ORR R1,     R1,     #0x1 <<27
        DMB
        MCR P15,    #0,     R1,     C1,     C0,     #1
        ISB

        ; Restore program counter

        MOV PC, LR

        .endasmfunc

    ;-------------------------------------------------------------------------------
    ; Disable core RAM ECC

        .def _CoreDisableRamEcc_
        .asmfunc

    _CoreDisableRamEcc_

        ; Disable BOTCM RAM PARECCENRAM[1]

        MRC P15,    #0,     R1,     C1,     C0,     #1
        MVN R0,     #0x1 <<26
        AND R1,     R1,     R0
        MVN R0,     #0x1 <<27
        AND R1,     R1,     R0

        DMB
        MCR P15,    #0,     R1,     C1,     C0,     #1
        ISB

        ;disable B1TCM  PARECCENRAM[2]

        MRC P15,    #0,     R1,     C1,     C0,     #1
        DMB
        MCR P15,    #0,     R1,     C1,     C0,     #1
        ISB

        ;PMNC Register to pass ERROR

        MRC P15,    #0,     R1,     C9,     C12,    #0

        ;Clear 4th bit of PMNC Register

        MVN R0,     #0x00000010
        AND R1,     R1,     R0
        DMB
        MCR P15,    #0,     R1,     C9,     C12,    #0
        ISB

        ; Restore program counter

        MOV PC, LR

        .endasmfunc

    --------------------------------------------------------------------------------------------------------------------------------

    Also, when i try to access watchdog i am unable to access.

    Any examples for stack configuration?

    Regards,

    Chitra

  • _coreInitStackPointer_ in sys_core.asm initialize the stack.

    Can you publish the whole project? I can not compile it without the .h and .inc file you try to include in this asm.

    Regards,

    Haixiao

  • Hi

    I can post the project. I am working for safety critical application. I will try to resolve the error for one more day.

    Regards

    Chitra

  • hi,

    Sorry for the late reply. I was on vacation. My CRC algorithm is working fine now.

    do yo have any file for assembly instructions? I want to have a look at the assembly instruction set. I will have to write some code for watchdog and other discrete which might need assembly coding. Also is there any example for GPIO mapping to discrete signals?

    Thanks

    Chitra

  • Arm instructions:
    http://infocenter.arm.com/help/advanced/indexList.jsp

    Search for "DDI0406B", After that, you needs to register and agree to the .... to download it.

    What do you mean "GPIO mapping to discrete signal"?

    Do you mean "how to set a GPIO high or clear a GPIO low"?

    Regards,

    Haixiao

  • hi

    Thank you for the link. I will download that.

    Currently I am implementing watchdog where i need to give trigger to watchdog using NHET or GPIO pins. I am trying to use NHET pins as GPIO pins and trying to write using NHET for which i may need support function. to make use of existing GPIO i think i can drive using GPIO registers available at port A and port B. but NHET write is little tricky. if you have some examples it would be great help.

    Regards

    Chitra