Hi,
Just a moment ago, I want to test the voltage between the NERROR pin(pin4 on J10) and the GND pin, while, some bad thing happened, one probe of the multimeter may be have a short across between 2 pins(I don't know which are they). Then,the leds on the board turned off suddenly, I just turn the power down.
When I turn on the power again, none of the led light. I thought maybe some components have burned out. I just test the 2A quick blow(F1) through the multimeter‘s diode files, the buzzer didn't ring.
When I link the miniusb with the PC only, the D10 and D11 shinning less than 1 secend and turn off, then D12 lights continuously.
Does it may have a serious consequences just like burn the chips? Can I fix it by myself?
Is it good to turn on the power again to test the voltage of the F1? Or, do you have any experience about that to find out the damaged component?
yong.