Other Parts Discussed in Thread: RM48L952, HALCOGEN, DP83640
The IwIP demo code does not mention how to make it work on the RM48L952 control card. Can we run this code on the control card and connect via Ethernet to a PC? Can anybody help me with these:
1. Are there any examples for using ethernet port on the control card?
2. Are there any step by step instructions as to what to do with the downloaded demo zip of the IwIP demo? I am not able to find any halcogen files at all and am not able to exactly figure out the directory structure in which to put the files to get a clean build!
3. If both above queries are answered positively, is there any example code or documentation how I can make it work with fixed IP address (not using DHCP)?
4. The wiki talks of HTTP server, UDP and echo server examples, but I find there is only the HTTP example in the unzipped code. Where can I find the UDP and echo server examples?
Any body out there have successfully used ethernet on Hercules paltform?