Other Parts Discussed in Thread: TUSB7320, TUSB1210
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TUSB7320, TUSB1210
Sachinkumar,
It is likely possible to be able to interface the two, but it would probably be a significant time investment. Is there good documentation on what and how the camera communicates over USB?
Hi,
Yes, We have provided with API from camera manufacture that is attached here.
We have checked camera hardware that includes "EZ-USB® FX2LP™ USB Microcontroller High-Speed USB Peripheral Controller" by cypress.
So, we are also thinking of "TUSB7320 USB 3.0 xHCI HOST CONTROLLER" as it is High speed host controller.
And Our main requirement of project is as mentioned that to program host controller board such that it will drive Camera (or EZ-USB® FX2LP™ USB Microcontroller) with some default setting after removing PC connection.
Thanks & Regards,
Sachin Panchal
Sachinkumar,
I apologize that I did not mentally connect "high speed" in the forum post body with the "USB 2.0" in the topic title. The Tiva parts do not support USB 2.0 High Speed mode (480 Mbps). The camera would have to connect at the much slow USB Full Speed (12 Mbps).
Also, if you want to use the TUSB3720, you will need a processor that has a PCI peripheral, which the Tiva parts do not. I don't know if the price or performance would be a good fit, but the Sitara processors have ULPI interfaces for USB 2.0 PHYs like the TUSB1210.