Other Parts Discussed in Thread: HALCOGEN
And else i,ve generated the code with halcogen, but i have an error
This is the C code:
/*
* main.c
*/
int main(void) {
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "sys_common.h"
#include "system.h"
/* USER CODE BEGIN (1) */
/* Include FreeRTOS scheduler files */
#include "FreeRTOS.h"
#include "os_task.h"
/* Include HET header file - types, definitions and function declarations for system driver */
#include "het.h"
#include "esm.h"
/* Define Task Handles */
xTaskHandle xTask1Handle;
/* Task1 */
void vTask1( void * pvParameters )
{
for(;;)
{
/* Taggle HET[1] with timer tick */
gioSetBit(hetPORT1, 17, gioGetBit(hetPORT1, 17) ^ 1);
vTaskDelay(100);
}
}
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
*
*/
/* USER CODE BEGIN (2) */
/* USER CODE END */
void main(void)
{
/* USER CODE BEGIN (3) */
/* Set high end timer GIO port hetPort pin direction to all output */
gioSetDirection(hetPORT1, 0xFFFFFFFF);
/* Create Task 1 */
if (xTaskCreate(vTask1, (const signed char *)"Task1", configMINIMAL_STACK_SIZE, NULL, 1, &xTask1Handle) != pdTRUE)
{
/* Task could not be created */
while(1);
}
/* Start Scheduler */
vTaskStartScheduler();
/* Run forever */
while(1);
/* USER CODE END */
}
/* USER CODE BEGIN (4) */
/* USER CODE END */
return 0;
}
but in the line with bracket:
void vTask1( void * pvParameters )
{ <-here there is an error 66 expected a " ;" main.c
for(;;)
what is the problem?
i attache the archive with programm.