Hello,
I am currently trying to create a PWM for the LM4F232H5QD that will control a solenoid.
In order to cause the solenoid to compress in, it needs to be at 17 volts for an extremely small amount of time, then it will go back to 0 volts.
I have a code set up but it seems like the only voltage I can get is around 3V. Is it possible for me to use a external DC supply to somehow raise the output voltage of the board, or is it not possible to run this solenoid on this board at all.
Thank you very much