Other Parts Discussed in Thread: UNIFLASH
Hello,
When I use UniFlash, which Motolora file should I change?
For example,
I change RM46x_demo_software.out to Motorola file
Which is correct either case1 or case2?
"condition": Device is configured in little endian mode(FFFFEA20h.0 bit =0)
・case1
Little Endian: "01_LE_RM46x_demo_software.m0"
address
S3 25 00000000 28BD01EA FEFFFFEA C0C701EA FEFFFFEA 1AC701EA FEFFFFEA B0F11FE5 B0F11FE5 D0
S3 25 00000020 2F696D61 6765732F 68657263 756C6573 5F657874 72616E65 745F6C61 6E64696E EC
・case2
Big Endian:"02_BE_RM46x_demo_software.m0"
address
S3 25 00000000 EA01BD28 EAFFFFFE EA01C7C0 EAFFFFFE EA01C71A EAFFFFFE E51FF1B0 E51FF1B0 D0
S3 25 00000020 616D692F 2F736567 63726568 73656C75 7478655F 656E6172 616C5F74 6E69646E EC
BTW, part of address is big endian, right?
if so, "00000020" is right?
And if "condition" is (FFFFEA20h.0 = 1) in fact it's big endian, should I download as case2 by UniFlash?
Regards,
JF