This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137 Boot loader

We are working on P2 board. For bootloader, it seems to be implemented through SPI, UART or CAN. For UART, is there any requiremnet for the port to be SCI(pin 38, 39 fro PGE) or LIN/SCI(pin 131, 132). I do not think there should, but double check. Also is there any I/O to be pulled down/up to be in the IAP mode or implementable by software. We just want to if there is any hardware requirement, update it in P2. Thanks,

  • Hello Huichun,

    There is a configuration header file "bl_config.h" for configuring the UART port, baud rate, address for application image, etc. You can use either port.

    Please refer to the user guide for the HW requirments. Thanks

    What is P2 board?

    Regards,

    QJ