Other Parts Discussed in Thread: RM48L952, HALCOGEN
Hello,
We are using the RM48 CNCD for a while now and we're quite happy with it. We have decided to use its MCU (RM48L952) in a design but the control card has RM48L952 in 337-Ball Grid Array (ZWT) while we are going to use the 144-Pin Quad Flatpack (PGE), so we want to ask if we can use CCS v5 and the XDS100 v2 emulator design (which will be built by us from the schematic here) to debug/program the MCU like we do with the control card? Furthermore, it seems the ZWT package doesn't have the pins N2HET1[21], GIOB[4], GIOA[4] or MIBSPI!NCS[3] which are available from the PGE package at the pins J13, G1,A6 and H4 from the PGE package, respectively. Unfortunately, RM48 Hardware Design Guide only discusses the ZWT package, so we once again would like to as if there are any other major/minor differences between these two packages in terms of programming, debugging or placing to the pcb? In other words, can we use, program, debug, route etc. it the way we do with the control card?
Thanks,
Asa