Hello Support,
Does RECEIVE Interrupt also occurs for DATA Frame for which FRAME Error Occurred in SCILIN Module with SCI Mode?
In essence, suppose for a DATA Frame, SCI Module detected FRAME Error at the end.
Will it generate both FRAME ERROR as well as RDY bits within SCIFLR Register?
Assume SCILIN Module being used in SCI Mode. Assume FE and RX Interrupts are enabled.
FE Interrupt mapped to INT0 and RDY Interrupt mapped to INT1 Levels of SCILIN Module.
Do I expect to have both interrupts for the Received DATA Frame being received for which FRAME Error took place due to some condition?
Thank you.
Regards
Pashan