Other Parts Discussed in Thread: TM4C123GH6PM, EK-TM4C123GXL
Greetings,
Some weeks ago arrived my first TI product, a Tiva C Series EK-TM4C123GXL LaunchPad with a TM4C123GH6PM MCU. To program it, I decided to use the Code Composer Studio IDE, along with TivaWare and all drivers necessary.
In fact, I'm having some success, as I'm able to run and edit all the examples codes on TivaWare software with just small problems. But, as I'm being unsuccessful trying to develop a project of my own, I would like the help of the community to find out what's happening. I'll illustrate the following problems with images, and you can take in account that I'm using the "Stellaris In-Circuit Debug Interface" as debugger.
First Problem:
This happens almost every project I try debbugging (in this case was the example project0). It runs normally, but when I order it to pause, this message appears. Doesn't cause any problems at least. The problem is when I order it to stop debugging: the device isn't stopped, it keeps running the code. Is it normal?
Same problem, now with the gpio_jtag example project.
Now the problem of halting the CPU, happening even when I try to pause. This happens sometimes, still didn't figure out exactly when. The project here was the example timers.
Now to my own project error. First of all, I tried creating a header file for initializing the PWM outputs for the three colors of the RGB Led and the Push buttons (left and right) on the PinMux software, then added the header to the program. The rest of the headers I tried to figure out by the examples. This problem specifically is the unability of the compiler to find one function, that I believe I already declared on the following header:
That's it, hope anyone around can help me ;)
Edit.: Images were inverted, now they're in the correct order ;)