Other Parts Discussed in Thread: RM48L952, HALCOGEN
Hello
I write software for the RM48L952. I use both N2HET modules:
- N2HET1 runs a custom het-assembler
- N2HET2 runs a het assembler generated by halcogen
I ported my existing N2HET application from HALCoGen 03.03.01 to 03.06.00.
Using the new generated files, both N2HET1 did not start. The reason is, that HALCoGen 03.06.00 configures both GCR registers to 0x01020001U instead of 0x01030001. The difference is bit 16 (CMS) which is set to "slave" for both N2HET modules.
Please allow the following questions:
- Where can I find documentation of the multi het sync feature? I did not find any except for the register description.
- Is it correct to configure the GCR of both N2HET to 0x01030001 to run both N2HET independently?
Best Regards
Flurin