I need a bytewide port from theTIVA launchpad. I am also using USB port in host mode, so that whole of Port D is not available. Which port should I use? I do not want to mix and use bits of different ports. Are the lines PA0,PA1 required for debugging/programming or can they be used in an application.
Regards