Other Parts Discussed in Thread: LM3S811, EK-LM3S8962
Hello,
I am currently running CCS 5.4.0.00091, ARM compiler 5.0.5 emulating with a Spectrum Digital XDS560v2 USB emulator with 5.2.0.08. I have a costume board with the TIVA TM4C1231D5PMI processor and a TI 20 Pin debug header. I have successfully debugged code on several of these boards. However, one board gives me the following error when I try to emulate.
Error connecting to the target:
(Error -1063 @ 0x0)
Device ID is not recognized or is not supported by driver. Confirm device and emulator configuration is correct, or update device driver.
(Emulation package 5.1.114.0)
I am unsure how to go about solving this issue as I am unable to connect to the device and swapping boards and retrying does not give the same error. Has anyone else seen this or have and insight as to how I may go about eliminating this problem?
Thanks,
Jeff